BX 3-BT
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
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
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
![]() |
This symbol is intended to draw special attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:![]() |
General symbol for "must do" |
![]() |
Wear eye protection |
![]() |
Wear hearing protection |
![]() |
Wear a hard hat |
![]() |
The Bluetooth® wordmark and the ![]() |
![]() |
Direct current (DC) |
![]() |
The power tool supports near-field communication (NFC) technology, which is compatible with iOS and Android platforms. |
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
If applied on the product, the product has been certified by this certification body for the US and Canadian markets according to the applicable standards. |
Product information

The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationType: BX 3-BT Generation: 02 Serial number:
Safety
General power tool safety warnings

Read all safety warnings and all instructions. Failure to follow the warnings and instructions may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference.
Work area safety
- Keep work area clean and well lit. Cluttered or dark areas invite accidents.
- Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
- Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
- Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
- Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
- Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
- Use personal protective equipment. Always wear eye protection. Protective equipment such as dust mask, non-skid safety shoes, hard hat, or hearing protection used for appropriate conditions will reduce personal injuries.
- Prevent unintentional starting. Ensure the switch is in the off‐position before connecting to battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
- Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
- Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
- Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
- If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
- Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
- Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
- Disconnect the battery pack from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
- Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
- Maintain power tools. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
- Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
- Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
- Recharge only with the charger specified by the manufacturer. A charger that is suitable for one type of battery pack may create a risk of fire when used with another battery pack.
- Use power tools only with specifically designated battery packs. Use of any other battery packs may create a risk of injury and fire.
- When battery pack is not in use, keep it away from other metal objects, like paper clips, coins, keys, nails, screws or other small metal objects, that can make a connection from one terminal to another. Shorting the battery terminals together may cause burns or a fire.
- Under abusive conditions, liquid may be ejected from the battery; avoid contact. If contact accidentally occurs, flush with water. If liquid contacts eyes, additionally seek medical help. Liquid ejected from the battery may cause irritation or burns.
- Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
Tacker safety warnings
- Always assume that the tool contains fasteners. Careless handling of the tacker can result in unexpected firing of fasteners and personal injury.
- Do not point the tool towards yourself or anyone nearby. Unexpected triggering will discharge the fastener causing an injury.
- Do not actuate the tool unless the tool is placed firmly against the workpiece. If the tool is not in contact with the workpiece, the fastener may be deflected away from your target.
- Disconnect the tool from the power source when the fastener jams in the tool. While removing a jammed fastener, the tacker may be accidentally activated if it is plugged in.
- Use caution while removing a jammed fastener. The mechanism may be under compression and the fastener may be forcefully discharged while attempting to free a jammed condition.
- When fastening electrical cables, make sure the cables are not energized. Hold the tacker only by insulated gripping surfaces. Use only fasteners designed for electrical cable installations. Inspect that the fastener has not damaged the insulation of the electrical cables. A fastener that damages the insulation of electric cables can lead to electric shock and fire hazards.
Safety instructions
Basic information concerning safety
Keep all safety precautions and instructions for future reference.
Requirements to be met by users
- Only authorized, appropriately trained persons may operate or service this tool.
- You and all other persons in the vicinity must wear suitable eye protection (ANSI Z87.1 (CAN/CSA Z94.3)) and a hard hat when the tool is in use.
- Wear hearing protection (ANSI S12.6 (S3.19)).
- Exposure to noise can cause hearing loss.
- Observe the information printed in the operating instructions concerning operation, care and maintenance.
- Stay alert, watch what you are doing and use common sense when operating a direct fastening tool. Do not use the tool when you are tired or under the influence of drugs, alcohol or medication. Take a break if you experience pain or feel unwell. A moment of inattention while operating tools may result in serious personal injury.
- Avoid awkward postures. Make sure you work from a safe stance and stay in balance at all times.
- Take breaks between working and do relaxation and finger exercises to improve the blood circulation in your fingers.
- Wear non-skid shoes.
- Keep the arms slightly bent while operating the tool (do not straighten the arms).
- Keep other people away from the working area, especially children.

- Use the right tool for the work you are carrying out. Do not use the tool for purposes for which it was not intended. Use it only as directed and when in faultless condition.
- Never leave a loaded tool unattended.
- Transport and store the tool in a secured toolbox.
- Always switch the tool off before cleaning, maintenance, changing the fastener guide, before work breaks and before storing the tool.
- When not in use, the tool should be unloaded and stored in a locked, dry place where it is inaccessible to children.
- Check the tool and the accessories for any damage. Check that moving parts function faultlessly, without sticking, and that no parts are damaged.
- All parts must be fitted correctly and fulfill all conditions necessary for correct operation of the tool. Damaged parts must be properly repaired or replaced by Hilti Service unless otherwise stated in the operating instructions.
- Before beginning work, check the working area (e.g. using a metal detector) to ensure that no concealed electric cables or gas and water pipes are present. External metal parts of the power tool may become live, for example, when an electric cable is damaged accidentally.
- Do not attempt to drive threaded studs into unsuitable materials.
- Unsuitable materials are glass, marble, plastic, bronze, brass, copper, insulating material, hollow brick, ceramic brick, thin sheet metal (< 4 mm) and cellular concrete. Driving a fastener into these materials may cause the fastener to break, splinter the material or to be driven right through.
- Pull the trigger only when the tool is fully pressed against the working surface at right angles.
- When driving fasteners, always hold the fastening tool at right angles to the working surface in order to prevent the threaded stud being deflected by the surface.
- Keep the grips dry, clean and free from oil and grease.
- Never drop the tool.
- Do not use the tool in places where there is a risk of fire or explosion unless the tool is specially approved for this type of use.
- Secure X-BT fasteners only in holes specially pre-drilled for this purpose.
- Keep the workplace tidy. Clear the work zone of objects that could cause injury.
- Untidiness in the working area can lead to accidents.
- Make sure that the working area is well lit and well ventilated.
- Do not tamper with or modify the tool or parts of it, especially the piston.
- Use only threaded studs of a type approved for use with the tool.
- Do not exceed the recommended maximum fastener driving rate (see the section headed "Technical data").
- If the tool has overheated, allow it to cool down.
- Do not dismantle the tool while it is hot. Allow the tool to cool down.
Careful handling and use of batteries
- Observe the special guidelines applicable to the transport, storage and use of lithium-ion batteries.
- Do not expose batteries to high temperatures, direct sunlight or fire.
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C (176 °F).
- Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your Hilti Service .
- If the battery is too hot to touch it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Contact Hilti Service .
Description
Overview of the product

- Fastener guide (X‑FG B3 series)
- Fastener driving depth adjuster
- Fastener guide locking catch
- Air vents
- Belt hook
- Trigger
- Grip
- Release buttons (also used to activate the charge status indicator)
- Li‑ion battery
- Status indicator
- On/off button
Intended use
The product is a hand-held, cordless fastening tool. It is designed for driving threaded studs (X-BT) into steel. Use only approved threaded studs in combination with the corresponding fastener guide.
The fastening tool, battery and threaded studs together form a technical entity. Use the Hilti threaded studs specially manufactured for the tool and the batteries and chargers recommended by Hilti . The fastening and application recommendations made by Hilti apply only when these conditions are observed.- The fastening tool is for hand-held use only.
- Misuse of the fastening tool must be ruled out. Misuse includes triggering without an X‑BT fastener inserted in the fastener guide.
Use only Hilti lithium‑ion batteries of the B 22 series with this product.
Use only Hilti -approved battery chargers to charge these batteries. More information is available from your Hilti Store or from www.hilti.group
Bluetooth
The product has a Bluetooth interface. Wireless communication via Bluetooth is possible as soon as the battery has been fitted and the fastening tool switched on at the on/off button.Data transfer continues for three hours after the tool has switched to standby mode or after the tool has been switched off at the on/off button.
To deactivate Bluetooth manually, press and hold down the on/off button for at least 5 seconds until the LED shows blue twice.
When the battery is removed, no further data are transferred.
Bluetooth is not available in all markets.
Bluetooth


Status indicator
The status indicator provides information about the status of the fastening tool.Status |
Meaning |
---|---|
Off |
The fastening tool is switched off |
The LED shows green. |
The fastening tool is switched on and ready for use |
The LED flashes green every 3 seconds. |
The fastening tool is in stand-by mode. Press the nose of the tool against the working surface to switch it on |
The LED flashes steadily green. |
The fastening tool is too hot or the battery has insufficient power; see “Troubleshooting” |
The LED flashes red. |
Malfunction; see “Troubleshooting” |
The LED shows red. |
Malfunction; see “Troubleshooting” |
The LED flashes yellow. |
Bring the fastening tool to Hilti Service. |
Indication of battery charge status
When one of the battery release buttons is pressed, the display indicates the battery’s state of charge.Status |
Meaning |
---|---|
All four LEDs show green. |
Charge status is 75 % to 100 %. |
Three LEDs show green. |
Charge status is 50 % to 75 %. |
Two LEDs show green. |
Charge status is 25 % to 50 %. |
One LED shows green. |
Charge status is 10 % to 25 %. |
One LED flashes green. |
Charge status is below 10 %. |
Items supplied
BX 3-BT fastening tool, X‑FG B3 series fastener guide, operating instructions.Other system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
Technical data
Fastening tool
Weight including battery |
B 22/2.6 Li-Ion (02) |
4.0 kg (8.8 lb) |
B 22/3.0 Li-Ion (01) |
4.1 kg (9.0 lb) |
|
B 22/4.0 Li-Ion |
4.2 kg (9.3 lb) |
|
B 22/5.2 Li-Ion (01) |
4.3 kg (9.5 lb) |
|
B 22/8.0 Li-Ion |
4.6 kg (10.1 lb) |
|
Threaded-stud length |
31 mm (1.2 in) |
|
Thread diameter |
8 mm …10 mm (0.3 in …0.4 in) |
|
Compression stroke |
12 mm (0.5 in) |
|
Contact pressure |
50 N …70 N (11 lbf …16 lbf) |
|
Application temperature (ambient temperature) |
−15 ℃ …50 ℃ (5 ℉ …122 ℉) |
|
Application temperature, threaded studs |
−10 ℃ …50 ℃ (14 ℉ …122 ℉) |
|
Recommended maximum driving rate |
650/h |
|
Rated voltage |
21.6 V |
Battery
Battery operating voltage |
21.6 V |
Ambient temperature for operation |
−17 ℃ …60 ℃ (1 ℉ …140 ℉) |
Storage temperature |
−20 ℃ …40 ℃ (−4 ℉ …104 ℉) |
Battery charging starting temperature |
−10 ℃ …45 ℃ (14 ℉ …113 ℉) |
Preparing the tool for use
Inserting the battery
- Charge the battery fully before using it for the first time.
- Push the battery into the product until it engages with an audible click.
- Check that the battery is seated securely.
Removing the battery
- Press the battery release buttons.
- Remove the battery from the tool.
Charging the battery
- Before charging the battery, read the operating instructions for the charger.
- Make sure that the contacts on the battery and the contacts on the charger are clean and dry.
- Use an approved charger to charge the battery.
Removing the fastener guide
- Switch off the fastening tool.
- Remove the battery.
- Remove the threaded stud from the fastener guide.
- Slide the fastener guide locking catch as far as it will go in the direction of the arrow.
- The fastener guide will be released.
- The fastener guide will be released.
- Remove the fastener guide.
Inserting the fastener guide

- Switch off the fastening tool.
- Remove the battery.
- Slide the fastener guide locking catch as far as it will go in the direction of the arrow and hold it in this position.
- Slide the fastener guide into the nosepiece until it engages with an audible click.
- Release the fastener guide locking catch.
- The fastener guide locking catch jumps to the middle position.
- The fastener guide locking catch jumps to the middle position.
- Grip and pull the fastener guide to check that it is securely seated.
Setting fastener driving depth

- Turn the fastener driving depth adjuster to the required driving depth.
- Check the quality of the fastening in accordance with the instructions supplied with the fasteners. Every time you make a change to the power level, you must use a new stud to do so.
Operation
Switching on the fastening tool

- Press the on/off button.
- The spring mechanism audibly builds up tension and the status indicator shows green.
- The spring mechanism audibly builds up tension and the status indicator shows green.
Switching off the fastening tool
- Press the on/off button.
- The spring mechanism audibly relieves its tension and the status indicator goes out.
- The spring mechanism audibly relieves its tension and the status indicator goes out.
Driving a fastener

- Switch on the fastening tool.
- Insert the threaded stud.
- Hold the fastening tool perpendicular to the working surface, center the fastener guide, loaded with a suitable threaded stud, over the pre-drilled hole and apply pressure to seat the fastener guide against the working surface.
- Drive the fastener by pulling the trigger.
- Lift the fastening tool completely clear of the working surface after driving a fastener.
Switching off Bluetooth
- Press the on/off button for at least 5 seconds until the LED shows blue twice.
- No further data transfer is possible.
- Bluetooth is not available in all markets
- No further data transfer is possible.
Care and maintenance
Care and maintenance
Care and maintenance of the tool- Switch off the fastening tool.
- Remove the battery.
- Remove the fastener from the fastener guide.
- Carefully remove any dirt that may be adhering to parts.
- Clean the air vents carefully with a dry brush.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Keep the battery free from oil and grease.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these may attack the plastic parts.
- Avoid ingress of moisture.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
- After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
Transport and storage of cordless tools
Transport- Switch off the fastening tool.
- Remove the battery.
- Remove the fastener from the fastener guide.
- Never transport batteries in bulk form (loose, unprotected).
- Check the tool and batteries for damage before use after long periods of transport.
- Store the tool and batteries in a place that is as cool and dry as possible.
- Never leave batteries in direct sunlight, near sources of heat or behind glass.
- Store the tool and batteries in a place where they cannot be accessed by children or unauthorized persons.
- Check the tool and batteries for damage before use after long periods of storage.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
The spring element is not tensioned; no status indication. |
The battery is empty. |
|
The battery is not fitted correctly. |
||
The spring element is not tensioned, the status indicator blinks green and 1 battery charge status LED blinks. |
The battery is empty. |
|
Battery temperature too low. |
|
|
The spring element is not re-tensioned, the status indicator blinks green and 4 battery charge status LEDs blink. |
The fastening tool has overheated. |
|
The spring element is not tensioned and the status indicator blinks red. |
The fastener guide is not fitted correctly. |
|
The spring element is not tensioned and the status indicator lights red. |
System fault |
|
Fastener driven at an angle. |
Too much contact pressure applied through the grip to the fastening tool. |
|
Fastening tool was angled off the driving axis when pressed against the surface. |
|
Disposal

Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
FCC statement (applicable in US) / IC statement (applicable in Canada)
The product complies with part 15 of the FCC Rules and RSS‑210 of the IC.Operation is subject to the following two conditions:
- This device shall cause no harmful interference.
- This device must accept any interference received, including interference that may cause undesired operation.