DWS 225 (01)
Original operating instructions
Information about the operating instructions
About these operating instructions
- Warning! Read and understand all accompanying documentation, including but not limited to instructions, safety warnings, illustrations, and specifications provided with this product. Familiarize yourself with all the instructions, safety warnings, illustrations, specifications, components, and functions of the product before use. Failure to do so may result in electric shock, fire, and/or serious injury. Save all warnings and instructions for future reference.
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
- The accompanying documentation corresponds to the current state of the art at the time of printing. Please always check for the latest version on the product’s page on Hilti’s website. To do this, follow the link or scan the QR code in this documentation, marked with the symbol
.
- Ensure that these operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
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
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
![]() |
This symbol is intended to draw special attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used additionally on the product:![]() |
Wear eye protection |
![]() |
Wear ear protection |
![]() |
Wear protective gloves |
![]() |
Wear light respiratory protection |
![]() |
Protection class II (double-insulated) |
![]() |
Diameter |
![]() |
Revolutions per minute |
![]() |
Revolutions per minute |
Product information
Hilti products are designed for professional use and may be operated, serviced and maintained only by trained, authorized personnel. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationRandom orbital sander DWS 225 Generation 01 Serial no.
Declaration of conformity

The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
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
- Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
- Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
- Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
- Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
- Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
- Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
- When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
- If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
- Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
- Use personal protective equipment. Always wear eye protection. Protective equipment such as a dust mask, non-skid safety shoes, hard hat or hearing protection used for appropriate conditions will reduce personal injuries.
- Prevent unintentional starting. Ensure the switch is in the off-position before connecting to power source and/or battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
- Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
- Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
- Dress properly. Do not wear loose clothing or jewellery. Keep your hair and clothing away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
- If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
- Do not let familiarity gained from frequent use of tools allow you to become complacent and ignore tool safety principles. A careless action can cause severe injury within a fraction of a second.
- Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
- Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
- Disconnect the plug from the power source and/or remove the battery pack, if detachable, from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
- Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
- Maintain power tools and accessories. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
- Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
- Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
- Keep handles and grasping surfaces dry, clean and free from oil and grease. Slippery handles and grasping surfaces do not allow for safe handling and control of the tool in unexpected situations.
- Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
Belt sander and drum sander safety warnings
- Hold the power tool by insulated gripping surfaces, because the sanding surface may contact its own cord. Cutting a "live" wire may make exposed metal parts of the power tool "live" and could give the operator an electric shock.
Additional safety instructions
- Use the power tool only when it is in perfect working order.
- Never tamper with or modify the power tool in any way.
- The power tool is not intended for use by persons who have received no special training. Keep the power tool out of reach of children.
- Always hold the power tool firmly with both hands on the grips provided. Keep the grips dry, clean and free from oil and grease.
- After installing the backing pad, always install the screw cap.
- Check the power tool, the backing pad, the supply cord and the connections at regular intervals for wear.
- Check the power tool’s supply cord at regular intervals and have it replaced by a qualified specialist if found to be damaged.
- Check extension cords at regular intervals and replace them if found to be damaged. Do not touch the supply cord or extension cord if it is damaged while working. Unplug the supply cord from the power outlet.
- In the event of an interruption in the electricity supply, switch the power tool off and unplug it from the power outlet to prevent an unwanted restart when power is restored.
Description
Product overview

- Sanding head
- Extractor
- Gripping surfaces
- Control panel
- Power cord socket
- Hose connector
- Backing pad
- Multi-purpose LED
- On/off button
- Speed indicator
- Increase/reduce speed
- Start/stop button
Intended use
The product is a hand-held, electrically powered random orbital sander. It is suitable for dry-sanding wood, wood-based materials, composites, varnishes, paints, plastics, plaster and filler compounds with wearing, replaceable sanding pads.
Possible misuse
- This product is not suitable for working on hazardous materials.
- This product is not suitable for working in a damp environment and use of the product for wet sanding is prohibited.
- Do not use backing pads with a nominal working speed lower than 8000 rpm.
LED indicators on the control panel

Status |
Meaning |
---|---|
A: Multi-purpose LED shows green |
AC supply connected. |
B: Multi-purpose LED shows green |
Power tool switched on and/or start/stop button pressed, speed indicator active. |
C: Multi-purpose LED flashes green/red |
Speed is increased/reduced; selected speed is indicated by the LEDs. |
D: Multi-purpose LED shows red |
Overtemperature warning. |
D: Multi-purpose LED quick-flashes green/red |
Voltage outside appropriate range. |
Sanding head

Items supplied
Random orbital sander, operating instructions.Other system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
Technical data
If the device is powered by a generator or transformer, the generator or transformer’s power output must be at least twice the rated input power shown on the rating plate of the device. The operating voltage of the transformer or generator must always be within +5 % and -15 % of the rated voltage of the device.DWS 225 |
|
---|---|
Weight in accordance with EPTA procedure 01 |
3.5 kg |
Speed |
4,000 /min … 8,000 /min (66.7 Hz … 133.3 Hz) |
Eccentric stroke |
5 mm |
Diameter, backing pad |
225 mm |
Use of extension cords

- Use only extension cords of a type approved for the application and with conductors of adequate cross-section. Otherwise the performance of the appliance may be affected and the cord may overheat.
- Regularly check the extension cord for damage.
- Replace damaged extension cords.
- When working outdoors, use only extension cords that are approved and correspondingly marked for this application.
Preparations at the workplace
Observe the safety instructions and warnings in this documentation and on the product.Positioning the sanding pad
- Unplug the supply cord from the power outlet.
- Select a suitable sanding pad and secure it to the backing pad. Make sure that the sanding pad is centered and securely seated against the backing pad.
Operation
Use of a ground fault circuit interrupter (residual current device, RCD) with a maximum tripping current of 30 mA is recommended.Switching on
- Press the on/off button.
- The multi-purpose LED shows green.
- The multi-purpose LED shows green.
Sanding
- Set the desired speed. To do this, use the "Increase/reduce speed" buttons as appropriate.
- Speed can be adjusted in the range from 4000 to 8000 rpm. The LED array indicates the set speed.
- Speed can be adjusted in the range from 4000 to 8000 rpm. The LED array indicates the set speed.
- Position the power tool with the whole of its sanding face on the surface to be sanded.
- Press the start/stop button.
- The sanding operation starts
- The sanding operation starts
- Applying moderate pressure, move the power tool steadily over the surface to be sanded.
Ending the sanding operation
- Lift the power tool clear of the surface being sanded before you end the sanding operation.
- Otherwise, the excessive speed could cause the abrasive to leave marks in the surface being sanded.
- Otherwise, the excessive speed could cause the abrasive to leave marks in the surface being sanded.
- Press the start/stop button.
Switching off
- Press the on/off button.
- Do not set the power tool down until the backing pad has come to a complete stop.
Care and maintenance
Care- Carefully remove stubborn dirt from the tool.
- Clean the air vents carefully with a dry brush.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as they can attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
- After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
Assembly modules

- Arbor and bearing module
- Sanding head
- Securing screw for sanding head
- Cap for screw
- Backing pad with securing screws
Changing the backing pad
Tools needed: 19 mm hex bit socket and Torx screwdriver.
- Disconnect the supply cord plug from the power outlet.
- Remove the screw cap.
- Remove the backing pad screw.
- Remove the old backing pad.
- Install the new backing pad positioned correctly on the spindle.
- Using the hex bit socket, tighten the backing pad screw to 10 Nm.
- Install the screw cap.
- Tighten the securing screw of the screw cap to 0.8 Nm.
- Tighten the securing screw of the screw cap to 0.8 Nm.
- Check that the backing pad is installed correctly and not tilted.
Changing backing pad and attachment pad
Tools needed: Plain screwdriver.
- Disconnect the supply cord plug from the power outlet.
- Remove the 8 recessed screws.
- Remove the attachment pad.
- Remove the old backing pad.
- Install the new backing pad positioned correctly on the spindle.
- Secure a new attachment pad.
- Re-install the 8 recessed screws.
- Re-install the 8 recessed screws.
- Check that backing pad and attachment pad are installed correctly and do not tilt.
Transport and storage
Transport- Make sure that the equipment is held securely throughout all transport operations.
- After transporting, always check all visible parts and controls for signs of damage and make sure that they all function correctly.
- Always store this product with the electric supply cable unplugged from the electricity supply.
- Store this product in a dry place, where it cannot be accessed by children or unauthorized persons.
- After a long period of storage, always check all visible parts and controls for signs of damage and make sure that they all function correctly.
Troubleshooting
Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
The multi-function LED flashes alternately red and green. |
The power tool is connected to a power outlet with the wrong voltage. |
|
The multi-function LED does not show when the power tool is switched on. |
The supply cord is not correctly connected to the power tool or the power outlet. |
|
The multi-function LED on the sander shows red, speed drops slightly. |
Excessive pressure applied to the power tool for a short time. |
|
The multi-function LED on the sander shows red and the speed of the sander drops to 4000 rpm while sanding is in progress. |
The temperature in the sander is too high. Excessive pressure applied to the power tool for a prolonged time. |
|
The seal on the backing pad does not work. |
Worn seal or faulty spindle bearing. |
|
The sander has stopped and the multi-function LED shows red. |
The power tool has switched to safe mode because the temperature was too high. |
|
Disposal

Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
Further information
China RoHS (Restriction of Hazardous Substances)
Extension cords