ST 1800 (01)
Original operating instructions
Information about the operating instructions
About these operating instructions
- Warning! Read and understand all accompanying documentation, including but not limited to instructions, safety warnings, illustrations, and specifications provided with this product. Familiarize yourself with all the instructions, safety warnings, illustrations, specifications, components, and functions of the product before use. Failure to do so may result in electric shock, fire, and/or serious injury. Save all warnings and instructions for future reference.
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
- The accompanying documentation corresponds to the current state of the art at the time of printing. Please always check for the latest version on the product’s page on Hilti’s website. To do this, follow the link or scan the QR code in this documentation, marked with the symbol
.
- Ensure that these operating instructions are with the product when it is given to other persons.
Explanation of symbols
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the operating instructions
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
The numbers in illustrations refer to important work steps or to components important for the work steps. In the text, the corresponding numbers draw attention to these work steps or components, e.g. (3) . |
![]() |
Item reference numbers are used in the overview illustration and refer to the numbers used in the key in the product overview section. |
![]() |
This symbol is intended to draw your special attention to certain points for handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:![]() |
The device supports near-field communication (NFC) technology compatible with iOS and Android platforms. |
![]() |
Protection class II (double-insulated) |
![]() |
If applied on the product, the product has been certified by this certification body for the US and Canadian markets according to the applicable standards. |
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
- Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
- Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
- Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
- Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
- Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
- Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
- When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
- If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
- Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
- Use personal protective equipment. Always wear eye protection. Protective equipment such as a dust mask, non-skid safety shoes, hard hat or hearing protection used for appropriate conditions will reduce personal injuries.
- Prevent unintentional starting. Ensure the switch is in the off-position before connecting to power source and/or battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
- Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
- Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
- Dress properly. Do not wear loose clothing or jewellery. Keep your hair and clothing away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
- If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
- Do not let familiarity gained from frequent use of tools allow you to become complacent and ignore tool safety principles. A careless action can cause severe injury within a fraction of a second.
- Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
- Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
- Disconnect the plug from the power source and/or remove the battery pack, if detachable, from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
- Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
- Maintain power tools and accessories. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
- Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
- Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
- Keep handles and grasping surfaces dry, clean and free from oil and grease. Slippery handles and grasping surfaces do not allow for safe handling and control of the tool in unexpected situations.
- Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
Safety warnings for screwdrivers and impact wrenches
- Hold the power tool by insulated gripping surfaces, when performing an operation where the fastener may contact hidden wiring or its own cord. Fasteners contacting a "live" wire may make exposed metal parts of the power tool "live" and could give the operator an electric shock.
Additional safety precautions for screwdrivers
Personal safety- Use the product and accessories only when they are in perfect working order.
- Never tamper with or modify the product or accessories in any way.
- Use auxiliary handles supplied with the product. Loss of control can cause personal injury.
- Always hold the product with both hands on the grips provided. Keep the grips clean and dry.
- Do not touch rotating parts – risk of injury!
- Wear suitable eye protection, a hard hat, ear protection, and light respiratory protection while the product is in use.
- Wear protective gloves when changing the accessory tool. Touching the accessory tool can result in cuts and burns.
- Wear eye protection. Flying fragments can injure the body and eyes.
- Dust produced by grinding, sanding, cutting and drilling can contain dangerous chemicals. Some examples are: lead or lead-based paints; brick, concrete and other masonry products, natural stone and other products containing silicates; certain types of wood, such as oak, beech and chemically treated wood; asbestos or materials that contain asbestos. Determine the exposure of the operator and bystanders by means of the hazard classification of the materials to be worked. Implement the necessary measures to restrict exposure to a safe level, for example by the use of a dust collection system or by the wearing of suitable respiratory protection. The general measures for reducing exposure include:
- working in an area that is well ventilated,
- avoidance of prolonged contact with dust,
- directing dust away from the face and body,
- wearing protective clothing and washing exposed areas of the skin with water and soap.
- Take frequent breaks and do physical exercises to improve the blood circulation in your fingers. High vibration during long periods of work can lead to disorders of the blood vessels and nervous system in the fingers, hands and wrists.
- Before beginning work, check the working area for concealed electric cables or gas and water pipes. External metal parts of the product could give you an electric shock or cause an explosion if you accidentally damage an electric cable or a gas or water pipe.
- Switch the product off immediately if the accessory tool jams. The product might twist off-line.
- Wait until the product stops completely before you lay it down.
Description
Overview of the product
- Chuck
- Protective sleeve
- Click connection between depth gauge and power tool
- Torque adjustment
- Control switch lockbutton
- Supply cord
- Control switch
- Forward / reverse switch
- Depth gauge adjustment
Intended use
The product described is a hand-held electric screwdriver for fastening profile metal sheets, metal sheets and sandwich panels in metal construction. The power tool is designed for driving and removing screws in drywall installation work.
It is possible to use a stand-up tool extension for driving collated screws.Main applications / torque settings
Application |
Screw type |
Diameter in mm |
Torque setting |
---|---|---|---|
Sheet metal to sheet metal |
S‑MD S‑MD S-MS |
4.2 4.8 4.8 |
1 - 2 1 - 8 1 - 8 |
Sheet metal to steel profile |
S-MD 51 + S-MD 21 S-MD 53 + S-MD 23 S‑MP 52 |
5.5 5.5 6.3 |
8 - 13 6 - 11 4 - 12 |
Sheet metal to steel beam |
S-MD 55 + S-MD 21 S‑MP 53 |
5.5 6.5 |
2 - 7 8 - 14 |
Sheet metal to timber |
S‑MP 53 |
6.5 |
14 - 18 |
Fiber-cement board on steel profile |
S-FD 03 |
6.3 |
6 - 12 |
Fiber-cement board on steel beam |
S-FD 05 |
6.3 |
12 - 15 |
Fiber-cement board on wood |
S-FD 01 |
6.5 |
12 - 18 |
Sandwich panel to steel profile |
S‑CD 63 |
5.5 |
2 - 7 |
Sandwich panel to steel beam |
S‑CD 65 |
5.5 |
2 - 9 |
Sandwich panel to wood |
S‑CDW 61 |
6.5 |
5 - 8 |
Items supplied
Metal construction screwdriver, ST‑DG 17 depth guage, operating instructions.Technical data
If the tool is powered by a generator or transformer, the generator or transformer’s power output must be at least twice the rated input power shown on the rating plate of the tool. The operating voltage of the transformer or generator must always be within +5 % and -15 % of the rated voltage of the tool.ST 1800 |
|
---|---|
Product generation |
01 |
Rated power input |
600 W |
Weight |
1.9 kg (4.2 lb) |
Speed (running under no load) |
0 /min … 1,900 /min |
Max. torque |
22 Nm (16 ftlbf) |
Chuck |
1/4" hex socket |
Protection class |
II |
Operating temperature |
−17 ℃ … 60 ℃ (1 ℉ … 140 ℉) |
Storage temperature |
−20 ℃ … 70 ℃ (−4 ℉ … 158 ℉) |
Operation
Preparations at the workplace
Observe the safety instructions and warnings in this documentation and on the product.Fitting the scaffold hook
- Push the scaffold hook onto the tool from the front.
- Turn scaffold hook into the desired position.
- Secure the scaffold hook by tightening the knurled thumb screw.
- Check that the scaffold hook is fitted securely.
Fitting the depth gauge
- Remove the protective sleeve.
- Fit the depth gauge.
Removing the depth gauge

- Remove the protective sleeve.
- Pull the depth gauge forward, away from the power tool.
Removing the protective sleeve

- Insert the tip of a screwdriver between the protective sleeve and the power tool.
- Release the protective sleeve by levering with the screwdriver.
- Pull the protective sleeve off toward the front of the tool.
Changing the bit
- Remove the depth gauge.
- Pull the sleeve back and hold it securely.
- Change the bit.
- Release the sleeve and allow it to slide forward.
- Fit the depth gauge.
Adjusting the depth gauge
Screw sealing washer compressed too much
If the screw sealing washer is compressed too much, turn the depth gauge to the right.Screw sealing washer is not compressed enough
If the screw sealing washer is not compressed enough, turn the depth gauge to the left.Types of work
Observe the safety instructions and warnings in this documentation and on the product.Switching on
- Press the control switch slowly all the way.
Activating continuous running mode
- Press the control switch.
- Press the lockbutton.
- To switch off when in continuous running mode, press the control switch.
- The lockbutton returns to its original position.
- The lockbutton returns to its original position.
Setting the torque

- Turn the adjusting ring to the desired torque setting.
Setting forward or reverse rotation

- Set the forward/reverse switch to the desired position.
Removing screws
Care and maintenance
Care- Carefully remove stubborn dirt from the tool.
- Clean the air vents carefully with a dry brush.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as they can attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
- After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
Transport and storage
- Do not transport electric tools with accessory tools fitted.
- Always unplug the supply cord before storing an electric tool or appliance.
- Store tools and appliances in a dry place where they cannot be accessed by children or unauthorized persons.
- Check electric tools or appliances for damage after long periods of transport or storage.
Disposal

Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.