C 7
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
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
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
![]() |
This symbol is intended to draw special attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols are used:![]() |
For indoor use only |
![]() |
Double insulated |
Product information

The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationCharger C 7 Generation 01 Serial no.
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Safety
General safety instructions

Keep all safety precautions and instructions for future reference.
The term “electric tool” used in the safety instructions refers to your mains-operated (corded) electric tool or battery-operated (cordless) electric tool.
Working area safety
- Keep your working area clean and well lit. Cluttered or dark working areas can cause accidents.
- Do not operate the power tool in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
- Keep bystanders, children and visitors away while operating the power tool. Distractions may cause you to lose control of the tool.
- The plug on the supply cord of the power tool must match the power outlet. Do not change the plug in any way. Do not use adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching power outlets reduce the risk of electric shock.
- Avoid body contact with earthed or grounded surfaces such as pipes, radiators, cookers, stoves and refrigerators. There is an increased risk of electric shock if your body is grounded.
- Do not expose the power tool to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
- Do not abuse the cord. Never use the cord to carry or hang up the power tool or to pull the plug out of the power outlet. Keep the cord well away from heat, oil, sharp edges and moving parts. Damaged or twisted supply cords increase the risk of electric shock.
- Use the battery charger only inside dry rooms. Water entering an electric appliance will increase the risk of electric shock.
Battery charger use and care
- To avoid injury, use the charger only to charge Hilti Li-ion batteries approved for use with this charger.
- The location at which the charger is used should be clean and cool but protected from frost.
- The charger must be able to emit heat while in operation. The air vents must therefore remain unobstructed. Accordingly, remove the charger from the toolbox. Do not operate the charger inside a closed container.
- Maintain the appliance carefully. Check to ensure that no parts are broken or damaged in such a way that the appliance may no longer function correctly. If parts are damaged, have the parts repaired before using the appliance.
- Use chargers and the corresponding batteries in accordance with these instructions and as is specified for this particular model. Use of chargers for applications different from those intended could result in hazardous situations.
- Recharge the batteries only with the chargers specified by the manufacturer. A charger that is suitable for a certain type of battery may present a risk of fire when used with other types of battery.
- When not in use, keep the battery and the charger away from paper clips, coins, keys, nails, screws or other small metal objects that could cause a short circuit at the battery terminals or the charging contacts. A short circuit between the battery terminals or charging contacts may cause injuries (burns) and result in fire.
- Under abusive conditions, liquid may be ejected from the battery. Avoid contact with the liquid. If contact accidentally occurs, flush with water. If the liquid contacts the eyes, also seek medical attention. Liquid leaking from the battery may cause irritation or burns.
- Make sure that the batteries suffer no mechanical damage.
- Do not charge or continue to use damaged batteries (e.g. batteries with cracks, broken parts, bent or pushed-in and/or pulled-out contacts).
Battery use and care
- Observe the special regulations and instructions applicable to the transport, storage and use of Li-ion batteries.
- Do not expose batteries to high temperatures, direct sunlight or fire.
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
- Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your Hilti Service .
- If the battery is too hot to touch it may be defective. In this case, place the product in a non-flammable location, well away from flammable materials, where it can be kept under observation and allowed to cool down. In this case, always contact your Hilti Service .
Additional safety instructions
Personal safety- Check to ensure that the charger is standing securely. A falling battery or charger may present a risk of injury to yourself and others.
- Do not touch the contacts.
- Batteries that have reached the end of their life must be disposed of safely and correctly to avoid environmental pollution.
- This appliance may be used by children 8 years of age or older and by persons with physical, sensory or mental disabilities or little relevant experience or know-how so long as they are supervised or they have received instruction on the safe use of the appliance and on the potential resulting hazards. Do not allow children to play with the appliance. Do not allow unsupervised children to clean the appliance or to perform maintenance tasks intended to be carried out by users.
- Do not wear jewelry such as rings or chains. Jewelry could cause a short circuit resulting in personal injury in the form of burns.
- Store power tools out of reach of children when not in use. Do not allow persons who are not familiar with the tool or these instructions to operate it .
- Do not touch the supply cord or extension cord if they are damaged while working. Disconnect the supply cord plug from the power outlet. Damaged supply cords or extension cords present a risk of electric shock.
- Never operate the appliance when it is dirty or wet. Dust (especially dust from conductive materials) or dampness adhering to the surface of the appliance may, under unfavorable conditions, lead to electric shock.
- Dirty or dusty power tools that have been used frequently for work on conductive materials should be checked at regular intervals by Hilti Service.
- Have the appliance serviced by a qualified repair person using only genuine Hilti spare parts. This ensures that the safety of the product is maintained.
Description
Product overview

- Charger
- Cord
- Battery compartment
- Operating status indicator
- Battery state of charge indicator
- Battery type B 7
LED display elements on the charger
Operating status indicator (1)
LED lights up green |
The charger is in operating condition. |
LED flashes red |
The battery is too cold (< 0 °C) or too hot (> 50 °C) and is not charging. The charger switches automatically into the charging mode as soon as the battery reaches the appropriate temperature. |
The LED lights up red LED does not light up. |
No power supply or the charger is defective. Unplug the supply cord from the power outlet and then plug the supply cord into the power outlet again. If the LED still does not light up, contact Hilti Service. |

LED flashes green |
The battery will be charged. |
LED lights up green |
The battery is fully charged. |
LED does not light up. |
The battery is not correctly plugged in or is defective. Remove the battery and insert it again in the battery compartment. If the LED still does not light up, contact Hilti Service. |
Intended use
The product described is a battery charger for Hilti Li-ion batteries of the type B 7. It is designed to be connected to power outlets providing an AC voltage (alternating current) of 220 to 240 volts.
The batteries approved for use with this product can be found in the technical data.Items supplied
Charger, operating instructions.Other system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group .
Technical data
Product properties
Cooling |
Cooling by convection |
Mains (AC) voltage |
220 V … 240 V |
AC frequency |
50 Hz … 60 Hz |
Battery |
Li‑ion |
Output voltage |
7.2 V |
Output power |
12.6 W |
Supply cord length |
≈ 2 m |
Weight |
0.775 kg |
Dimensions (L x W x H) |
152 mm x 102 mm x 58 mm |
Control |
Electrical charging monitoring and control via microcontroller |
Protection class |
Protection class II (double insulated) |
Temperature specifications
Battery charging starting temperature |
−10 ℃ … 45 ℃ |
Storage temperature |
−20 ℃ … 40 ℃ |
Ambient temperature for operation |
−17 ℃ … 60 ℃ |
Battery charging times
Voltage |
Battery type |
Charging time |
---|---|---|
7.2 V |
B 7/1.5 Li-Ion |
≈ 45 min |
7.2 V |
B 7/2.0 Li-Ion |
≈ 60 min |
Operation
Switching the charger on
- Plug the supply cord into the power outlet.
- LED 1 on the charger lights up green.
- LED 1 on the charger lights up green.
Charging the battery
- Make sure that the contacts on the battery and the contacts on the charger are clean and dry.
- A list of the batteries approved for use with this product can be found at the end of this document.
- A list of the batteries approved for use with this product can be found at the end of this document.
- Push the battery into the interface of the charger. Check that the encoding of the battery and charger interface match.
- Charging begins automatically after insertion of the battery in the charger. The state of charge indicator on the battery is deactivated during charging.
- Charging begins automatically after insertion of the battery in the charger. The state of charge indicator on the battery is deactivated during charging.
Inserting the battery
- Charge the battery fully before using it for the first time.
- Push the battery into the battery holder until it engages with an audible click.
- Check that the battery is seated securely.
Removing the battery
- Press the release buttons on the battery.
- Pull the battery out of its holder in the device.
Care and maintenance
Care- Carefully remove any dirt that may be adhering to parts.
- Clean the air vents carefully with a dry brush.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these may attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
- After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
Disposal

In accordance with the European Directive on waste electrical and electronic appliances and its implementation in conformance with national law, electrical and electronic appliances that have reached the end of their life must be collected separately and returned to an environmentally compatible recycling facility.
RoHS (Restriction of Hazardous Substances)
Click on the links to go to the table of hazardous substances: qr.hilti.com/2076993.There is a link to the RoHS table, in the form of a QR code, at the end of this document.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.